Other Parts Discussed in Thread: DP83867E
Hi team,
My customer made 1000BASE-T compliance test with his own board which is equipped with DP83867IR.
As a result, the A and B peak voltage test failed.
The customer searched DP83867 compliance test fail inquiries in E2E and he found below two inquiries.
The customer thinks it seems that responses are done individually and the answer is not disclosed
in E2E thread.
The customer believes that the answers will be hints for his test failures.
So the customer wants to know these answers.
Can you provide the answers to the customer?
Or should the customer post individually as a new inquiry?
Please let me know.
E2E thread title:
・[DP83867IR] compliance test is failed
・DP83867E: Fail the A and B peak voltage test of 1000m Ethernet compliance test
Best regards,
Fumio Nakano