Hi,
I have questions about DP83822 Ethernet Compliance test of 100BASE-TX.
In DP83822, there are "Compliance Test Register(COMPT), address 0x0027".
I thought I need to configure this COMPT register, but in the following application report of DP83822,
there are no information about COMPT register.
********************************************************
DP83822 IEEE 802.3u Compliance and Debug
www.tij.co.jp/.../snla266.pdf
********************************************************
From above application report, it seems I only need to set following DP83822 registers
for 100BASE-TX Compliance Test:
- BMCR(Basic Mode Control Register), address 0x0000
- PHYCR(PHY Control Register), address 0x0019
- PHYRCR(PHY Reset Control Register), address 0x001F
Q1.Do I need to set COMPT register for 100BASE-TX compliance test?
Q2.If answer of Q1 is "yes", when and what value do I need to set to COMPT register?
Q3.If anwser of Q1 is "no" , what is the purpose of COMPT register?
best regards,
g.f.