Hi
I have questions about start up sequence of DP83867E.
Q1.
According to the Figure 1 in datasheet, 32 MDC clock cycle is described.
Must the 32clock cycle be required after power-up?
Or is it just showing first read/write operation?
Q2.
In three supply mode, there is supply sequence that VDDA1P8 must be stable within 25ms after VDDA2P5 is ramped up but any other sequnece is not required. Is it possible to apply VDDA1P8(1.8V) and VDDA2P5(2.5V) when VDDIO and VDD1P0 is not powered?
Q3.
I could not get the meaning of NOTE described on Page 97 in the datasheet.
What is that note saying? VDDA1P8 can be ramped up before VDDA2P5? But I think it is inhibited by Talbe 107.
Q4.
There is no power sequence requirement in two-supply mode.
The NOTE mentioned in Q3 is not applied in two-supply mode. Is my understanding correct?
BestRegards