When I am running the DS280DF810 Ibis AMI model in Sigrity SystemSI and I include the supplied 100 Ohm input termination to the retimer I don't get any output. Is there something I'm missing with the setup? When I do not include the termination the output of the retimer is a square wave and at the final receiver it's an eye diagram again.