Other Parts Discussed in Thread: DA8XX, 66AK2E05
Tool/software: Linux
Hi,
We are using TI DP83867IS phy at our developmemt board of K2E type. I am able to configure and use this PHY at u-boot.
Now i want to use this at LINUX as well, but even after adding this to device tree not able to use the PHY.
[ 24.352823] serdes PLL not locked
[ 24.871627] netcp-1.0 2620110.netcp: phy not found on slave 1
[ 24.881475] net eth1: module open failed
[ 25.187608] random: crng init done
[ 27.177168] serdes PLL not locked
[ 27.696699] netcp-1.0 2620110.netcp: phy not found on slave 0
[ 27.707509] net eth0: module open failed
I want to clarify that, In K2E EVM the SGMII Reference clock is 156.25MHz but our custom board has 125MHz clock. PHY is connetced in SGMII mode on board, i read somewhere that SGMII is not supported for this PHY at linux and i confirmed this from driver as well as there is no configuration is written at linux.
Please let me know that what all changes are required as per the above requirements.
Thanks
Prince