I have two questions of the different reading in the datasheet:
1. I see page 45 from this datasheet. The page contained Table 4 "Strap Resistor Ratios". Now if you look at page 51, you see RX_D4 connected to ground via 2.49 kOm resistor. What is the selected mode for RX_D4? On 50 page i see "RX_D4 = Strap Mode 4". Is it mistake?
2. On Page 30 section 8.4.1 i see this text "The RGMII Disable strap (RX_D6) determines the default state of the MAC interface. The RGMII Disable strap corresponds to the RGMII Enable (bit 7) in the RGMIICTL register (address 0x0032). When RGMII mode is disabled, the DP83867 operates in GMII mode."
if the "RGMII Disable strap" = 0 the device uses RGMII mode, but if the "RGMII Enable bit" = 0 the device uses RMII mode. I think "RGMII Disable strap not corresponds to the RGMII Enable" or am i not right?
Please, answer of my questions.
Best regards, Ruslan