Hi Team,
My customer feedback an issue of DS125DF1610.
When the device didn't power up,but there is input signal at RX pin(the dc was 1.2V),then they can see 450mV leakage voltage at VDD pins.
The schematic was shown as below.Could you help check is there any internal connection between RX pin and VDD pin which will be a voltage path when device not power up and is there any risk for device in such condition?
Best Regards,
Nick Dai