This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: DP83822I register configuration

Part Number: DP83822I

Hi team,

My customer is using our DP83822 in their new project and they are developing the software to configure the DP83822 registers. The interface between the DP83822 and the processor is RMII and they use the RJ45 connector.

They have realized the communication function but there's a strange phenomenon about the DP83822. When they use a computer to apply a "ping" command, it succeeded. But when they use another computer with a different brand, the "ping" command failed. I wonder if this problem is related to the register configuration. Do you have any comment on this issue?

By the way, do you have the source code for configuring the register? If you have, could you please send it to so I can share with customer and let them check their configuration.

Best regards,

Wayne

  • Hi team,

    Here's a new situation. When customer is debugging the DP83822, they found that the link will sometimes fail. After checking the code, they found that the link failure is related to a sentence used to read registers. When they remove this sentence and don't read any register, the link works fine for a long time. But when they add this sentence to read some registers and no matter which register they read, the link cannot maintain stable and it will sometimes fail. Do you have any comment on this issue? Thank you.

    Best regards,

    Wayne

  • Hi Wayne,

    That is very interesting. Do you have the phy schematic you can share? And a layout of the phy?

    Best regards,