• Resolved

DP83867E: SFD timing adjustment?

Part Number: DP83867E

The datasheet of the DP83867E devices says in section 8.3.2 "The exact timing of the pulse can be adjusted through register. Each increment of phase value is an 8-ns step.". I could not find a "register" that allows to change the timing of the pulse. I guess what is meant is that the real TX_SFD to RX_SFD timing requires correction which can be read from registers as is described in 8.3.2.1?