New design using DP83867ERZ.
No special strapping options, all are default/open.
The device does not attempt auto-negotiation at power up as expected, I've reviewed all the basic stuff and haven't found anything wrong.
When again review the strapping option pins, specifically for RX_CTRL, it would seem that MODE 1 is N/A and has a special note "(1) Only Mode 3 and 4 are valid for RX_CTRL. Mode 1 and 2 are not applicable and should not be used"
Since MODE 1 is the default strapping option (ie: no reisistors), then how can this be N/A?
Further NOTE for RX_CTRL is:
Strap modes 1 and 2 are not applicable for RX_CTRL. The RX_CTRL strap must be configured for strap mode 3 or strap mode 4. If the RX_CTRL pin cannot be strapped to mode 3 or mode 4, bit[7] of Configuration Register 4 (address 0x0031) must be cleared to 0
Since bit 7 of Configuration Register 4 is defined as RESERVED and reads back '0', does the note about clearing this really apply.
Was/Is there a bug/errata in regards to the strapping option on the RX_CTRL pin (if I read between the lines it seems there is)
Thanks
Jeff