Other Parts Discussed in Thread: DS125DF1610
Hello,
I am exploring the FIR and VOD settings of the DS125DF1610 and I am stalling a bit on the normalization step.
In SigCon Architect, when I select a "Driver VOD setting" (High level page, Tx FIR/VOD section), I can see pre-set values being updated for Pre/Main/Post cursor taps, DEM and DRV_SEL_VOD as well as a "Calculated VOD". However, the value "Driver VOD setting" and the "Calculated VOD" are sometimes very different: differences range from 0.09% for 350 mVpp (calculated VOD = 350.312 mVpp) to 19% for 650 mVpp (calculated VOD = 527.67 mVpp)! I measured the VOD at the output of the DS125DF1610 for all possible settings and the measurement follows the "Driver VOD setting" quite closely: differences below 5% for all but one setting.
How come the calculated VOD is off if the setting is correct? If the calculation is off, does that mean the normalization process (when I click on "Normalize Taps") may be off too?
Say I want to set up a VOD that is not in the provided list, like 625 mVpp. How do I normalize the taps? Is there a formula linking the Pre/Main/Post cursor taps, DEM and DRV_SEL_VOD that I could follow so that if I want 625 mVpp with Pre tap = -7 and Post tap = -7 I can extract the Main tap value out of it?
Thank you,
--
RD