This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83849IF: RJ45 to FIBER adaptor

Part Number: DP83849IF

Hi,

have been asked about adding 10/100 Mb ethernet  transport between a couple of units, the connection between wich can be only by means of fiber optics.

I'm evaluating having a standard, commercial router with SFP cage  at one side of the link, and a fiber to rj45 adapter board at the other.

I may go for commercially available boards for this side too, but have some space constrains that seem impeding implementation of the smaller ones i googled out.

The question is: will a custom board built as follows solve? Or should it mandatorily include other logic like memories, MACS, etc.?

-1 SFP attached to say CHANNEL 1 FX TRX port of one (DP83849IF, DP83849I-) phyter series chip

-1 x RJ45 (with magnetics) attached to say CHANNEL 2 TX TRX port of the same chip

- MRII interfaces of the channels cross connected

- a small MCU for configuration (wether not feasible simply by strapped pins options)

Thanks Francesco