This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TUSB9261 firmware release notes / change log

Prodigy 20 points

Replies: 4

Views: 984

Dear support-team,

I noticed that there's a new default firmware version 1.05 for TUSB9261 available. Currently, we are using version 1.04 in our embedded device (TUSB9261 is connected via USB3.0 hub to a SigmaDesigns SX6). Now I like to know what have changed from v1.04 to v1.05 to decide whether to update or not. I have downloaded and 'installed' the firmware package already, but unfortunately there's no change log included.


Background: We have complains about the TUSB9261 sometimes not being recognized by the SX6 while the hub is there. However, these cases are very seldom and at the moment I can't say which part is responsible: SX6 host, hub chip (SMSC 5534b) or the TUSB9261. But maybe the firmware update can help?


Thanks and best regards, Christian.

  • I would also like to know what the v1.05 change history is because I can no longer get UAS to work with this version, this worked in v1.04.
  • Hello Christian,

    These are the changes implemented in the FW 1.05

    v1.05 - 03Oct2014
    -----------------
    - Updated fixed format sense info for ATA PASS-THROUGH commands per SAT-3r02 spec.
    - Increased delay at the end of usb_hal_disconnect() to 500ms to ensure device disconnect is detected by host.
    - Added parsing of SATA model number info to extract Vendor ID instead of using SAT-3 spec Vendor ID of "ATA" for standard inquiry response. If the drive is not ready, "TI-DSG TUSB9261" will be returned for vendor and product ID.
    - Forced UAS to be disabled regardless of external descriptors until compatibility issues can be resolved.
    - Updated SW license terms and added manifest.
    - Updated build scripts to use CCS v5.1.8 toolchain.

    Regards,
    Roberto.
  • In reply to Roberto Diaz:

    Thank you Roberto, that helps to make the decision.

    Best regards, Christian

  • In reply to Roberto Diaz:

    Hi Roberto-san,

    Could you explain about the following questions regqarding the FW1.05?

    v1.05 - 03Oct2014
    -----------------
    - Increased delay at the end of usb_hal_disconnect() to 500ms to ensure device disconnect is detected by host.
         --> What is the parameter of "usb_hal_disconnect()"?
                      My customer has evaluated TUSB9261 with the FW of v1.04 since 2014.
                      They have a concern whether they should update FW from v1.04 into v1.05.

    - Updated SW license terms and added manifest
         --> Where should we check to confirm contents of the above things? 
                       They want to confirm what are updated.

    Thank you.

    Best Regards,

    Koshi Ninomiya

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.