This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TCA6424A: TCA6424A standby mode

Guru 12335 points

Part Number: TCA6424A

I could not figure from the datasheet of the TCA6424A,how the device enters into standby mode.

I can see that after reset assertion the registers and FSMs are initialized and all ports are configured as high impedance inputs, but is it standby mode? What should be the current consumption on this state?

 The reset feature and low power is a main consideration for choosing the IO expander on this project.

  • Hello Eli,

    For this device, "standby mode" is just considered to be the state where all the ports are configured as inputs, are pulled up, and no toggling is occurring on the I2C bus. In this condition, the worst-case current consumption is 3 uA.

    Please let us know if you have any other questions.

    Regards,
    Max
  • Guru 12335 points

    In reply to Max Robertson:

    Hello Max,Thanks
    Can you tell me what should be the current consumption in a situation similar to the one you described,
    except the ports (configured as inputs) will be externally pulled down?
    This is our preferred “standby” way.
  • In reply to eli:

    Eli,

    This should be the same in terms of standby current. What would cause higher currents would be holding the input ports at an intermediate voltage between ground and VCCP.

    Max

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.