This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4E02B04: I have a question about the part TPD4E02B04

Part Number: TPD4E02B04

I have a question about the part TPD4E02B04.

I am going to use TPD4E02B04 for displayport 1.3.
TPD4E02B04 datadheet says it can be used for displayport 1.3
There is an article called Supports High Speed Interfaces up to 10 Gbps in the 1 Features section of the datasheet.
What is this?
8K UHD display (7680 × 4320), 30 Hz Can I use this part if I am using it?

And displayport 8K UHD (7680 × 4320), 60 Hz Are there any parts that support it?

please answer about my question.

Thank you.

2 Replies

  • Hello,

    I will have to get back to you about this.

    Regards,

    Cameron

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

  • In reply to Cameron Phillips:

    Hello,
    I believe the the data rate is 35Gbps right?
    Is this split up between several data lanes?
    35Gbps is too high for the TPD4E02B04
    Regards,
    Cameron

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.