This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD4E1U06: tidu515a

Part Number: TPD4E1U06

Hi Sir 

I saw TPD4E1U06 used on tidu515a

1. I saw ESD test can pass level 4 ,is it correct?

2. Have any solution is better than TPD4E1U06 and could be used on Ethernet application ?

Thanks 

  • Hello,
    Yes the TPD4E1U06 has IEC 61000-4-2 level 4 protection.
    This device will work in ethernet applications. We do have plans to release parts with higher protection for Ethernet very soon. If you would like more information email me at c-phillips@ti.com
    Regards,
    Cameron

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.