This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN65HVD1782-Q1: Driver differential output voltage magnitude at 3.3 V VCC

Part Number: SN65HVD1782-Q1

Hello,

 

In the SN65HVD1782-Q1 datasheet MIN and TYP |VOD| are not provided for a load of 100 Ohm, a VCC of 3.3V and a temperature of 85C. Can you give me those values?

 

Thank you

 

Francesco

  • Francesco,

    Unfortunately we don't have any characterization data with 100Ohm load and Vcc=3.3V. I can get the estimate based on the simulation for your reference. But it's not real characterization. Do you think it's good enough for your purpose?

    Regards,

    Hao

  • In reply to Hao L:

    Hello Hao,

    Simulation results are sufficient. Is it something I can simulate myself? IF yes can you tell me how?

    Thank you

    Francesco

  • In reply to Francesco Ricci:

    Francesco,
    You can find the device ibis model here (http://www.ti.com/product/SN65HVD1782/toolssoftware). There are several simulators you can use, for example HyperLynx. The setup is straightforward. This app note (http://www.ti.com/lit/an/slaa747/slaa747.pdf) might be helpful. Please let me know if this route works for you.
    Regards,
    Hao

  • In reply to Hao L:

    Thank you!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.