This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPD1S414: MAX9940 Cross Reference

Part Number: TPD1S414

Hi,

My customer is looking for a cross reference to MAX9940.  I had recommended the TPD1S414 as it was the closest solution I saw.  However, the customer is using an open drain single wire interface which signaled by MCU pulling the line low.  TPD1S414 has an undervoltage lock out and they are concerned this would be triggered each time the line gets pulled low.  Can you confirm if there would be any issue with using the TPD1S414 or provide a alternative cross to the MAX9940?

I can provide more details on the application offline if needed.

Thanks,

Chuchen

  • Hi Chuchen,

    Maybe we need more details. Could you tell us how the TPD1S414 is connected with MCU?
    UVLO is from Vbus_con pin and it should be power flow versus signal connection. Thank you.

    Best regards,
    Feifei

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.