This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

AM26C32: Alternative Pin Layout to be foot-print compatible with TX?

Part Number: AM26C32

Dear Team,

our customer intends to build a modular PCB that could be used as TX or RX board. To do that, they were wondering if if there is a RX available that has the same pin layout like a TX.

Example: The AM26C32 has
1 - 1A input
2 - 1Y output
3 - 1Z output

A similar TX has:

1 - 1B input
2 - 1A input
3 - 1Y output

Does any TX device exist that has:

1 - 1Y output
2 - 1_ input
3 - 1_ input

Thanks and best regards
Martin

Does this post answer Your question? Please mark it with the "Verify Answer" button.

  • Martin,
    Unfortunately all quad receivers have the same pin out on 1/2/3. Please let me know if I can help in other ways.
    Regards,
    Hao
  • In reply to Hao L:

    Hao,
    thanks for the answer. I will keep you posted if we have another question & content selection.
    Best Regards
    Martin

    Does this post answer Your question? Please mark it with the "Verify Answer" button.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.