This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TRSF3232: Output Driving Current

Part Number: TRSF3232

Hi,

May I know where can find TRSF3232 Output Driving Current?

Due we need to connect long cable(~10m)  and need to check signal quality again.

Thanks.

Regards,

Eric

  • Eric,

    The maximum current that the device will output is given in the driver short-circuit output current (IOS) specification. What is probably more relevant to your question, though, would be the output voltage (VOH and VOL) and output slew rate (SR) or data rate specifications. These are defined with a worst-case RS-232 load of 3 kOhm as well as a variety of load capacitance values in order to simulate the parasitic capacitances that would be introduced by various capacitances.

    If you have any further questions on this please just let me know.

    Regards,
    Max

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.