This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD4S214: OVP & OCP device for USB OTG

Guru 24585 points

Replies: 1

Views: 344

Part Number: TPD4S214

Hi Team,

My customer is looking for OVP & OCP device for USB OTG.
The requirement is the following.

- over voltage protection up to 28V VBUS
- OVLO (output overvoltage lockout) threshold is 6~7V
- current limit is adjustable more than 1.5A

There is TPD4S214 however current limit is up to 1.2A.
Is there another solution for this requirement?

Best Regards,
Yaita / Japan disty

  • We do not have a device that will provide all of the functionality of the TPD4S214 and more than 1.5A of current limit range.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.