This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD2EUSB30A: Suitable for Ethernet Interface

Intellectual 2985 points

Replies: 3

Views: 566

Part Number: TPD2EUSB30A

Hello,

We need to protect a 10/100 ethernet interface.   At present the TPD2EUSB30A is in the circuit, but we're concerned the the reverse breakdown voltage may not be high enough.

Would the TPS2EUSB30 (Non A) be more suitable for this interface?

Don

  • Don,

    You are correct that the reverse breakdown might not be high enough. Do you know if you are using a current controlled or a voltage controlled PHY? Is your signal going to 5V or 3.3V?

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

    If this answers your query, Please click "This resolved my issue" button.

  • In reply to Cameron Phillips:

    Appreciate the timely response,

    We are targeting the DP83848I. The PHY is being powered by 3.3V.

    Don
  • In reply to Donald Schelle90399:

    The TPD2EUSB30 would be more suitable than the A version but I would say that the TPD2E2U06 would be better suited than either of them. Or if you need a 4 channel device the TPD4E05U06 would work as well.

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

    If this answers your query, Please click "This resolved my issue" button.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.