This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPD4E05U06: TPD4E05U06DQAR SATA INTERFACE

Prodigy 100 points

Replies: 1

Views: 248

Part Number: TPD4E05U06

Hi,

Is it advisable to use TPD4E05U06DQAR for SATA interface?

in the datasheet it is mentioned as for eSATA it can be used, but in my design I have SATA interface along with USB 3.0, USB 2.0, SD CARD, HDMI, where I'm using TPD4E05U06DQAR ESD chip. so for BOM optimization will this be used for SATA also.

thanks

Sathiya

  • Sathiya,
    If you are referring to 6Gbps SATA then yes the TPD4E05U06 can be used. However this is a unidirectional device so if you are AC coupling the signal you will need to put the device before the AC coupling capacitors.
    Also make sure that the common mode signal is 5V or less (I believe it is 3.3V)

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

    If this answers your query, Please click "This resolved my issue" button.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.