This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TVS1400: Can TVS1400 withstands a 1hr overvoltage test

Prodigy 20 points

Replies: 1

Views: 120

Part Number: TVS1400

Hi Sir,

    If I use TVS1400 at a power input. Then having a over voltage test like 22V power input for an hour.

    Will the device burn down? 

    Thanks!

  • Hello,

    Yes more than likely. The TVS1400 is not for DC applications it is for transient events. Theoretically if you have an extremely low current source then it could survive but at 22V the TVS1400 is in highly conductive mode and will take as much current as possible.

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

    If this answers your query, Please click "This resolved my issue" button.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.