This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD4S012: Junction Temperature

Intellectual 1135 points

Replies: 3

Views: 213

Part Number: TPD4S012

Hello All,

Is the below a true statement for the TPD4S012DRYR device.

In general ESD protection devices are assuming negligible current draw due to leakage and therefore Tj = Ta

  • Hello,
    The junction temperature is not the ambient temperature during an ESD event. However because the ESD pulse is so short none of the heat dissipates beyond the die itself.

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

    If this answers your query, Please click "This resolved my issue" button.

  • In reply to Cameron Phillips:

    Thanks Cameron,
    So for this device would the junction and ambient temperature be the same?
  • In reply to Daniel Vasher:

    Daniel,
    During normal operation yes it is extremely close due to the minimal power dissipation. However the maximum ambient temperature for the device is not the maximum junction temperature.

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

    If this answers your query, Please click "This resolved my issue" button.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.