This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

PCI2050B: Number of connected slave

Mastermind 7555 points

Replies: 2

Views: 98

Part Number: PCI2050B

Hello,

I would like you to ask about below.

--

Q1, Is it possible that PCI2050B connect up to 16 slave device as shown below ?

Q2. According to datasheet, it seems that Parallel data bus is 32 bit. So this device support only 32bit bus, right (Not support 64 bit) ?

--

Best Regards,

  • Ryuuichi machida,

    Q1, Is it possible that PCI2050B connect up to 16 slave device as shown below ?

    Multiple PCI2050B can can create a Bus Hierarchy  to achieve 16 "PCI slaves" (See Figure 3−4 and Figure 3−1 in datasheet for better understanding). One PCI2050B can only connect up to nine secondary bus masters at a time on the secondary PCI bus. 

    Q2. According to datasheet, it seems that Parallel data bus is 32 bit. So this device support only 32bit bus, right (Not support 64 bit) ?

    This is correct. 

  • In reply to Malik Barton57:

    Hello Malik-san,

    Thank you for your reply.

    Understood.

    BR,

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.