This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 87
Part Number: PCI2050B
Hello,
I would like you to ask about below.
--
Q1, Is it possible that PCI2050B connect up to 16 slave device as shown below ?
Q2. According to datasheet, it seems that Parallel data bus is 32 bit. So this device support only 32bit bus, right (Not support 64 bit) ?
Best Regards,
Ryuuichi machida,
Multiple PCI2050B can can create a Bus Hierarchy to achieve 16 "PCI slaves" (See Figure 3−4 and Figure 3−1 in datasheet for better understanding). One PCI2050B can only connect up to nine secondary bus masters at a time on the secondary PCI bus.
This is correct.
In reply to Malik Barton57:
Hello Malik-san,
Thank you for your reply.
Understood.
BR,