This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 88
Part Number: TLK2711-SP
Hello,
for example below,
A simple and effective protocol can be implemented as follows.• K28.5 D5.6 // k code, data• K28.5 D5.6 // k code, data• K28.5 D11.5 (SOF optional and user definable)• Dxx Dxx (Transmitted packet. Repeat for packet depth.) //WHAT IS THE DATA SIZE without (k code) comma ???????• Dxx Dxx (Packet CRC if desired)• K28.5 D5.6 // k code, data• K28.5 D5.6 // k code, data• K28.5 D11.5 (SOF optional)
Regards,
In reply to Kirby Kruckmeyer96848:
In reply to Bernard Bertrand: