This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SN75DP159: Application about SN75DP159

Intellectual 2440 points

Replies: 3

Views: 80

Part Number: SN75DP159

Hi team,

My customer are looking for a device can be a bridge for the DP++ to HDMI and can support 4K application.

Can the SN75DP159 support this application?

Lacey

Thanks a lot!

  • Lacey

    SN65DP159 can supports data rate up to 6-Gbps per data lane to support Ultra HD (4K × 2K / 60-Hz) 8-bits per color high-resolution video and
    HDTV with 16-bit color depth at 1080p (1920 × 1080 /60-Hz).

    It is designed for DP++ to HDMI.

    Please refer to this link to the ref schematic: www.ti.com/.../sllu224b.pdf.

    Thanks
    David
  • In reply to David (ASIC) Liu:

    Hi David,
    Is there DP159RSBEVM available in TI store that customer can apply for?
    They have a new project that want to use the SN65DP159, so they want to firstly test the performance using the EVM.
    Lacey
    Thanks a lot!
  • In reply to Lacey Lin:

    Lacey

    I checked, it looks like the EVM is stock.

    Thanks
    David

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.