This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SN65DSI85: Signal skew

Genius 11745 points

Replies: 5

Views: 150

Part Number: SN65DSI85

Hi,

For MIPI input, customer's DP to MIPI bridge IC is designated for to two separated LCD for left & right eye, so that there is a skew(tSK) 1.88us between mipi port 00 & mipi port 10

May I know if it is ok for SN65DSI85?

Thanks!

Antony

  • Hi Antony,

    If that is less than 9 DSI HS clock cycles as the image depicts, then it should be fine. 

    Regards,

    I.K. 

  • In reply to I.K. Anyiam:

    Hi I.K.,

    Thanks for your reply. 

    But since customer project is dual panel 1280*720, with DSI clock cycle is around 4.4ns.

    Their DP to MIPI bridge IC skew could achieve 1.88us which is larger than 9*cycles…

     

    What would be the risk for this ?  Anyway to solve or improve it?

     

    Thanks!

     

    Antony

     

  • In reply to Antony Lin:

    Hi Antony,

    They should try and reduce the skew so that it is within datasheet recommendations. 1.88us is very excessive.

    Regards,

    I.K. 

  • In reply to I.K. Anyiam:

    HI I.K.,

    May we know what could the exactly application issue from such a long skew?  No display?  Display with lots of noise.....?

    Thanks!

    Antony

  • In reply to Antony Lin:

    It can result in those display anomalies, yes.

    Regards,

    I.K. 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.