This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD2S703-Q1: Can I use TPD2S703-Q1 for CC pins of USB Type-C?

Guru 15995 points

Replies: 2

Views: 106

Part Number: TPD2S703-Q1

Hi Team,

 

Can I use TPD2S703-Q1 for CC pins of USB Type-C?

 

We need Short-to-VBUS protection on CC pins IC of Automotive grade.

However, we can’t find Automotive grade IC in TI lineup.

Therefore, we would like to know whether TPD2S703-Q1 is usable for CC pins.

 

Regards,

Kanemaru

  • Hi Kanemaru,

    The TPD2S703-Q1 can't be use for protect the CC pin  as the max OVP protect threshold is 4.5V. In the type C SPEC the CC line voltage can up to 5.5V, So it can't meet the application requirement. 

  • Guru 15995 points

    In reply to Michael Tan:

    Hi Michael-san,

    Thank you for your prompt reply and detail information.

    I greatly appreciate your cooperation.

    Regards,

    Kanemaru

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.