• TI Thinks Resolved

DP83849C: RJ45 Loopback

Prodigy 150 points

Replies: 4

Views: 86

Part Number: DP83849C

Dear DP83894c Experts,

I would like to run a RJ-45 loopback test; that is with a plug on the RJ45 that loops the TX data to RX.

Post reset, are there any registers that I must configure in order to see a successful loopback of an ethernet frame?

Kind regards,

Rocco

  • With Auto-Neg set to 100M, you shall see the link is up and data transfer shall go thru.

    Regards,
    Geet

  • In reply to Geet Modi:

    Hi,

    I am closing this thread. Incase you need further assistance, kindly open new thread and provide reference to this thread.

    Regards,

    Geet

  • In reply to Geet Modi:

    Hi Geet,

    I proceeded with the RJ-45 loopback before answer arrived and it worked. It works without auto-negotiation. It works with 100 bits/sec set. I guess this is not abnormal , yes ?

    Kind regards,

    Rocco

  • In reply to Rochus:

    Tx and Rx are seperate and you can setup link using external loop back.

    Regards,
    Geet