This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983: TPS65983 SCH Check

Intellectual 540 points

Replies: 1

Views: 52

Part Number: TPS65983

Dear All:

    Please help check TPS65983 SCH and support firmware bin file, thank you!

Request: PD support 20V/5A output.

exta-v10-20190812-1451.pdf

1 Reply

  • Hi,

    I want to check if you are asking about TPS65983 or TPS6583B.

    I can make a general reply that you should download the TPS6598x configuration tool to create customized device firmware.

    There are additional restrictions on the TPS65983B device.

    Regards,

    Scott

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.