• TI Thinks Resolved

DS90UB954-Q1: DS90UB954-Q1

Prodigy 215 points

Replies: 9

Views: 209

Part Number: DS90UB954-Q1

I have a DS90UB954 connected remotely to a pcb with two DS90UB953.

There are two possible I2C addresses for the 953 – 0x18, 0x19.

RX Port 0 is connected to 0x18 and RX Port 1 is connected to 0x19.

There is an accelerometer on the pcb also has the same two possible address 0x18 and 0x19.

I have selected 0x19 and connected it to the 953 (0x18) on RX Port 0.

I am using aliased addressing. BCC_CONFIG REG 0x58 is set to 0x5D

On most occasions I can correctly read the accelerometer ID register (0x33) without any problem.

However, sometimes the device powers up in such a way that the value returned is (0x00)

I scope both the 954 I2C bus and the 953 I2C bus. The correct data is output by the accelerometer (0x33) but it isn’t transferred correctly to the 954 I2C where it appears as (0x00)

I am wondering if there is some problem with the addresses being so close in value.  I can't see why this should be but this is the only device which ever causes an issue.

The transaction always appears on the 953 I2C bus which implies that it is being recognised as external to the 953 - at least in the Maser -> Slave direction.

Any help would be much appreciated.

Thanks

Paul

  • Hello Paul,

    Can you help us understand a little bit more about the order of events? Which devices power up in what order? Also what mode is being used for the 953/954? Synchronous?

    Best Regards,

    Casey 

  • In reply to Casey McCrea:

    Hello Paul,

    Any feedback?

    Thanks,

    Casey 

  • In reply to Casey McCrea:

    Hi Casey,

    Our power-up sequence is firstly 954 on the local board followed by the remote 953 - powered across the cable by a supply generated on the 954 pcb.

    Our operational mode is CSI synchronous.

    This occurrence of this issue is so infrequent that I can't be exactly sure of sequence with regards to connecting USB, power to USB2ANY, PoE to 954 pcb.

    Is this a known issue?  And if so, is it related to power sequencing?

    Please let me know if you require any more information.

    Thanks

    Paul

  • In reply to paulmcw:

    Hey Paul,

    There is no known issue persay but please pay careful attention to the power up sequencing of each part to ensure it meets the datasheet requirements. Failure to meet rail order/PDB sequencing can cause some strange issues on rare occasions. I have seen similar symptoms when the PoC voltage has a glitch which causes the power rails going to the serializer to glitch and come back up in the wrong order for example. Also see our video here on power rail sequencing for more information: https://training.ti.com/power-sequencing-fpd-link-devices?cu=1134310

    Best Regards,

    Casey 

  • In reply to Casey McCrea:

    Hi Casey,

    Thanks for the prompt reply.  I watched the video

    The 954 uses external 1v8 and the internal 1v1 LDO.  The PDB pin has 10k,10uF connected to 1v8 to hold in reset while the power comes up.

    The 953 uses external 1v8 only.  The PDB pin has 10k,10uF connected to 1v8 to hold in reset while the power comes up.

    They would appear to meet all the power-up requirements.

    The issue I'm seeing seems to be determined at power-up - once in the state only a repower appears to correct it.

    Do you have any thoughts as to whether the issue is likely to be in the 953 or the 954?

    Would a hard reset be likely to correct the issue? I haven't seen it often enough to be able to test.

    Is it permissible to have the PDB pin high at power up and then to issue a hard reset (driving a low pulse on the PDB pin) before using the device.  Or is it strictly necessary to meet the power-up conditions for PDB?

    Thanks

    Paul 

  • In reply to paulmcw:

    Hi Paul,

    Can't say right now where the issue exists. The hard reset is not required, it is explaining how long you should wait before applying the hard reset on the PDB. Although, do you get better results when you do a hard reset? 

    - Just to clarify, this issues is occurring rarely? or is it consistent?

    - Have you tried to provide a different address alias to the SER and DES? If so, what were the results?

    - Also, I was reading through the post and you mentioned 0x33? for clarification, is this the data you were expecting out of the accelerometer? or is this another address?

    - I noticed you are running the Back Channel at 25Mbps? Is that intentional? We recommend running at 50Mbps as the default setting for 953/954 sync mode, so BCC_CONFIG = 0x5E

    Regards,
    Mandeep Singh

  • In reply to Mandeep S:

    Hi Paul,

    Do you have any other questions regarding this post?

    Regards,
    Mandeep Singh

  • In reply to Mandeep S:

    Hi Mandeep,

    Apologies for being slow to get back.  To answer your previous questions.

    I have only seen the issue on 2 occasions.

    Both times a repowering was used to clear it - I didn't do a hard reset.

    The DES doesn't use an alias Address (does it?)

    The ALP profile seems to force the Alias for the two SER at 0x0C and 0x0D.(7 bit)

    So I haven't tried any alternative addresses.

    The 0x33 is the data that is output by the accelerometer to the 953 I2C (observed on the oscilloscope).  This is not transferred successfully to the 954 I2C. On that bus I observe 0x00.

    We sending the video data across a long twisted.  Required bandwidth is less than 2G, so reach is extended by running the back channel at 25M rather than 50M.  Are we correct in understanding that the forward channel rate is directly controlled by the back channel rate.

    My follow up questions:

    Is it recognised that closely related addresses can cause a problem?  I think I might have read that on one occasion but can't find the reference now.

    The fact that the problem has only been seen with a slave address (0x19) which matches the address of the 2nd 953 (although it  is actually connected to the 1st 953 with a 0x18 address) does lend weight to the possibility.

    I presume there is no issue with operating at a back channel rate of 25M.  Or is there? The device allow the rate to be configured.  What problem could result in not running at 50M?

    Thanks

    Paul

  • In reply to paulmcw:

    Hi Paul,

    Per i2c protocol, the LSB is a reserved bit and is used as an indicator for a read or write. Perhaps this explains why you are getting issues when you use the device ID 0x19. See

    2) There's no issues if you use 50MHz or 25MHz but your understanding is right. In Sync mode, the back channel will directly effect the Forward channel rate.