• Resolved

DP83825I: dp83825

Prodigy 70 points

Replies: 5

Views: 162

Part Number: DP83825I

Hi Team,

The system structure is using STM32F4 MCU + DP83825I, MDIO communication is norma,Why does the indicator light on the router not turn on and the linkstatus in the dp83825 register is 0 when connected to the router through RJ45?

thinks


The state value of 0x00 is 0x3100

The state value of 0x04 is 0x01E1

The state value of 0x00 is 0x5002

The state value of 0x00 is 0x8000

the router can successfully link up when connected to another 100Mbps device

-Regards