• TI Thinks Resolved

DS90UB948-Q1: I2C interface

Expert 1300 points

Replies: 1

Views: 34

Part Number: DS90UB948-Q1

Hi,

The serializer is DS90UB947-Q1 and the deserializer is DS90UB948-Q1. I want to control 948 using 947's I2C. The I2C signal transmits through LVDS signal and the I2C signal can output through 948's I2C interface.

Can I get the function? If so, could you please tell me how to configure 948 and 947?

Thanks.

Kevin Xiong

  • Yes, this can do. Kevin.

    As one of key features is I2C over FPD-Link communication, pls see below app. note i2c over FPD-Link? here you can get how the I2C is communicated over FPD-Link and how to set the reg. (pass-through and alias slave ID / slave ID) ,.thanks.

    www.ti.com/.../snla131a.pdf

    regards,

    Steven