Dear all,
I want to connect a LCD display with parallel RGB, to HDMI (for those interested, I want to connect it to a Raspberry Pi in the future). First of all the LCD is a TFT LCD from a photoframe, with not a standard parallel RGB pinout (e.g. HSYNC/VSYNC/CK). Instead it has some other (for me unknown pins.). The pinout is in the datasheet (page 8, I've marked the pins I don't know about). 2450.CLAA080MB0GCW.pdf. My idea is to use the TFP401A to connect the HDMI to the RGB interface.
My question is, how do I connect these two together(the chip and the display). Or is this not possible?
If this is possible, which pin do I connect to what?
I've made a overview of what I'm planning to make (The device being a computer or a Raspberry Pi for example):
Thank you in advance,
Robert Grootjans