This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD1E6B06: ESD protection on SPI lines

Genius 4765 points

Replies: 2

Views: 804

Part Number: TPD1E6B06

Hi,

ESD protection on SPI lines

We are considering using ESD protection elements for SPI lines.
Is there no problem using TPD1E6B06?

best regards

                                                                                                                                                                                                                            

  • Cafain-

    That device should work properly for SPI protection. Because SPI is a 5V max line with a low bandwidth, the 6pF capacitance and 6V working voltage will effectively protect the line.

    Thanks,

    Alec

  • In reply to Alec Forbes:

    Hi, Alec-san

    Thank you for your support.
    We expect to pass on system level ESD testing.

    best regards

    cafain

                                                                                                                                                                                                                                

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.