This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SN65DPHY440SS: MIPI retimer to support MIPI Camera 2GHz CLK speed

Expert 4205 points

Replies: 2

Views: 347

Part Number: SN65DPHY440SS

Dear experts,

Would you let me know if there is proper part for retimer to get MIPI CAMERA 2GHz CLK ? 

DPHY440 can support only up to 750MHz .. Also, I want to know if HDMI or DP retimer can be used as MIPI retimer..

Thanks for your answer in advance.

Thanks,

JH.

  • Hello Jung-Ho Seo,
    At this point, we do not have a MIPI retimer that supports 2Gpbs.
    The physical layers of HDMI and DP have several differences than the physical layer of MIPI D-PHY. An HDMI or DP retimer is not suitable for a MIPI camera.

    Regards
  • In reply to Joel Jimenez0:

    Hi Joel,
    Thanks for kind answer.
    Regards,
    JH.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.