Hi, Team
I want to enable the internal pattern generation feature of DS90UB940 to test the display module, and I configure the DS90UB940's register as following(use the default timing configuration)
Write 0x03 to address 0x65 PGCFG
Write 0x11 to address 0x64 PGCTL
but the the display module can not get the video output from DS90UB940. Maybe the pattern feature doesn't work.
How should I configure the register to enable the pattern feature?
How can I judge if the pattern feature works well? (When use extern video input from DS90UB949, I can judge the LOCK bit).
And to be clear, when connect DS90UB949 to DS90UB940 and make DS90UB949 generate pattern, the display is ok.
Thank you!