Hi,
Can P82B96 be used in the following configuraion ?
Best regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Kato,
The P82B96 is meant to be used in a pair and not in this kind of configuration. What I mean by this is, if each slave is on a different board and the master is also on a different board then each board needs its own P82B96 to talk to another P82B96. In this case, your master needs one as well.
I've redrawn what I was talking about below. Please note I did not draw the pull up resistors but they do need to be there.
Thanks,
-Bobby
Hi Bobby-san,
For Q1 and Q2, please see the following comments and give me your advice.
Q1:
VCCM = 3.0V ~ 5.5V
VCCB = 12V
VCCS = 3.0V ~ 5.5V
Master device VCC = 3.0V ~ 5.5V
Slave devices VCC = 3.0V ~ 5.5V
* Not be fixed
Q2:
The master device and the slave devices are on different boards.
In addition, there is a possibility to mount "the slave device #0 ~ #2", "the slave device #3 ~ #5", the slave device #6 ~ #8" and "the slave device #9 ~ #11"on different board.
Best regards,
Kato
Hi Max-san,
Thank you for your support.
I understood and will contact you if I get additional questions from our customer.
Best regards,
Kato