I have a question about the part TPD4E02B04.
I am going to use TPD4E02B04 for displayport 1.3.
TPD4E02B04 datadheet says it can be used for displayport 1.3
There is an article called Supports High Speed Interfaces up to 10 Gbps in the 1 Features section of the datasheet.
What is this?
8K UHD display (7680 × 4320), 30 Hz Can I use this part if I am using it?
And displayport 8K UHD (7680 × 4320), 60 Hz Are there any parts that support it?
please answer about my question.
Thank you.