Other Parts Discussed in Thread: TIDA-01323
Tool/software: Linux
I am debug-ing DS90UB964 and DS90UB913 control channel.
the current condition:
1)Less than 20% probability to correctly write 913 registers
2)964‘s status reg have error.
0x4D's val is:0x33/0x51(two board have diff val)
0x4E's val is:0xe5
3)try digital reset,but i could not see 0x01 reg's reset bit self clean
write_reg(0x01, 0x01)-----could not see the val become 0 again
Please help to see this issue,thank you very much.