Hi all
Would you mind if we ask TPD12S016?
Our customer uses TPD12S016 and has the same connection between TPD12S016 and AM57XX like as the attachment file.
20180614_TPD12S016.pdf
We have the question the difference of low level voltage(VIL) between CEC_A/HPD_A and SDA_A/LS_OE.
On the customer's board;
CEC_A / HPD_A : 0.4V
SDA_A / LS_OE : less than 0.1V
On the datasheet P6, the VIL(Max) value of CEC_A and SDA_A is the same as 0.082×VCCA.
However, there is the differece.
Does it mean cause of sink capability at AM57XX?(I2C usually drive 3mA, GPIO pin less than 3mA??)
If you have some advice, could you let us know?
Kind regards,
Hirotaka Matsumoto