This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD4E02B04: Is this ESD Protection Diode for USB Type-C pass any level of IEC 61000-4-6 international standard ?

Part Number: TPD4E02B04

Hi! I have a few questions about TPD4E02B04 ESD Protection Diode for USB Type-C,

1.Is this ESD Protection Diode pass any level of IEC 61000-4-6 international standard ?

2.Can you briefly explain is it important for  USB Type-C protection device to pass this standard(IEC 61000-4-6) ?

3.If it's important  , is there any recommend  ESD protection devices for USB Type-C which included this protection(IEC 61000-4-6) ?

Thanks you very much!

 

  • Hello,
    The TPD4E02B04 alone is not useful for the IEC 61000-4-6 conducted immunity standard.
    I’m order to comply with this standard you need the entire system. On its own it does not really help your system to be compliant except for its capacitive effects.
    Regards,
    Cameron

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.