This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983: firmware request for TPS65983 for AR SP BPD PCIE REV2P6

Part Number: TPS65983

Hi Helper,

I have a thunderbolt 3 design with  TPS65983 in sink (Device) side. and follow the internal reference design thunderbolt 3.0. Refer below details please:

   We use TPS65983 external MOS path to drawing VBUS power from host, so ours only as endpoint. And we use the TBT controller is Intel Alpine Ridge JHL6340, which shared external flash is W25Q80DVSSIG, TPS65983 share this flash. The reference is “AR SP BPD PCIE REV2P6_FINAL”.

Can you help to check and share the matched PD firmware to me? 

 

Thanks.

Brian Xiao