This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DS90UB947-Q1: paired with ds90ub926 use GPIO7_REG for PWM dimming

Intellectual 1950 points

Replies: 1

Views: 432

Part Number: DS90UB947-Q1

Hi team,

Can we use GPIO7_REG for PWM dimming when pairing with ds90ub926?

We followed below setting 947(0x11=0x33), 926 (0x21=0x55), this configuration works for 925+926 but failed for 947+926. Besides, interrupt and video display works well, PWM frequency is 20kHz.

Is there anything wrong with my configuration? Does 947 support this kind of usage with 926?

Dongbao

  • Pls check d/s, GPIO_REG7 is used for local GPIO pin only. to enable the remote transmission function, you can set the pin34 (I2S_WC) work at I2S mode. regards, Steven

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.