Hi, all.
We have some problems with FPD channel layout at our card, so I was asked to investigate this issue, and I have some questions.
The FPD channel is operated at COAX mode.
1) Why should the "RIN-" trace be loosely coupled to the "RIN+" trace? Why can't we route the FPD as a 100ohm differential microstrip/stripline between the deserializer and the connector? After all, the RIN of the deserializer is designed to be differential, isn't it?
2) Alternatively, why can't we place the termination resistor of 50ohm close to the deserializer right after 47nF capacitor? Some tutorial says, it should be placed close to the connector?
3) In case we route the FPD at the outer layer, and the next layer is ground, should we moat more layers below the FB1? (The stack-up is L1(sig) - L2(gnd) - L3(sig) - L4(gnd))
4) Is it so critical to route the "RIN+" trace at the opposite side from the connector? The wavelength at 4Gbps (2GHz) using FR-4 is about 75 mm, while the stub is about 2-3 mm. I understand we want to do the best, but will this stub significantly degrade the signal?
Sorry for my English and many questions.
Best regards
Alex