Other Parts Discussed in Thread: ALP
Hi folks,
I use a TDA2P+Fusion Board to create a link to an AR0220 sensor including an UB953. On board there are two UB960.
After I connect the sensor to a cam port (connected with U1) the UB960 didn't recognize a FPD-III link. Only If I change the BC frequency to 25 Mbps the UB960 recognize the link.
But if I connect the sensor to a radar/cam port (connected with U2) the UB960 recognize a FPD-III link instantly with a BC frequency of 50 Mbps.
I also changed the Power selcetion (5V / 12V) of every instance. But there is no difference.
What's the difference of the UB960? Why U1 didn't work with a BC frequency of 50 Mbps? Although U1 should work with a BC frequency of 50 Mbps.
Best regards,
Alex