Other Parts Discussed in Thread: THVD1450, SN65HVD35
Hello,
I have a question about transmission distance of RS-485.
Is there a correlation for the transmission distance and Vcc voltage of THVD1452?
Is the following recognition right?
Transmission distance(@Vcc=5V) > Transmission distance(@Vcc=3.3V)
Or, is it related to the signal level?
Best Regards,
itabi